WeldBuilderWeldLocation Enumeration¶
NXOpen.CAE.WeldBuilder.WeldLocation is an alias for NXOpen.CAE.WeldBuilderWeldLocation
-
class
NXOpen.CAE.
WeldBuilderWeldLocation
¶ Bases:
object
Represents the options for type of operation
Enum Members
Enum Member Enum Member Description Point Creates a weld at locations specified using points File Creates a weld at locations specified in an input file Edge Creates a weld at locations on an edge Node Creates a weld at locations specified using nodes -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-