WeldBuilderPointOnEdgeType Enumeration¶
NXOpen.CAE.WeldBuilder.PointOnEdgeType is an alias for NXOpen.CAE.WeldBuilderPointOnEdgeType
-
class
NXOpen.CAE.
WeldBuilderPointOnEdgeType
¶ Bases:
object
Represents the options for specifying number of weld points on an edge
Enum Members
Enum Member Enum Member Description ByNumber Specify the number of weld points to be created on an edge ByDistance Specify the distance between weld points created on an edge ByPattern Specify the distance between weld points as a pattern -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-