TransientResultsReductionBuilderNoData Enumeration

NXOpen.CAE.TransientResultsReductionBuilder.NoData is an alias for NXOpen.CAE.TransientResultsReductionBuilderNoData

class NXOpen.CAE.TransientResultsReductionBuilderNoData

Bases: object

No data options

Enum Members

Enum Member Enum Member Description
Skip
ZeroFill
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.