ThicknessPlotContoursBuilder Class¶
-
class
NXOpen.CAE.
ThicknessPlotContoursBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ThicknessPlotContoursBuilder
builder which can be used to generate a plot of aNXOpen.CAE.SimBC
in the graphics area.This is limited to
NXOpen.CAE.SimBC
objects in the active solution.CAE.SimBcPlotContoursBuilder.CreatePlotObject()
returns a plot objectNXOpen.CAE.NxBcPlotContours
whoseNXOpen.CAE.NxBcPlotContours.PlotContour()
plots contour. To create a new instance of this class, useNXOpen.CAE.NodeElementInfoManager.CreateThicknessPlotContoursBuilder()
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreatePlotObject | Returns NXOpen.CAE.ThicknessPlotContours object |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetMeshesToPlot | Sets NXOpen.CAE.Mesh objects to plot. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
CreatePlotObject¶
-
ThicknessPlotContoursBuilder.
CreatePlotObject
¶ Returns
NXOpen.CAE.ThicknessPlotContours
objectSignature
CreatePlotObject()
Returns: Return type: NXOpen.CAE.ThicknessPlotContours
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetMeshesToPlot¶
-
ThicknessPlotContoursBuilder.
SetMeshesToPlot
¶ Sets
NXOpen.CAE.Mesh
objects to plot.Signature
SetMeshesToPlot(pMeshTags)
Parameters: pMeshTags (list of NXOpen.CAE.Mesh
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
ThicknessPlotContoursBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.