ThickenMeshBuilder Class¶
-
class
NXOpen.CAE.
ThickenMeshBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ThickenMeshBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateThickenMeshBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ElementType | Returns the element type |
SelectMesh | Returns the select mesh |
Tag | Returns the Tag for this object. |
ThicknessValue | Returns the thickness value |
Methods¶
Method | Description |
---|---|
AutomaticThicknessValue | The creation of automatic thickness value |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ElementType¶
-
ThickenMeshBuilder.
ElementType
¶ Returns the element type
-------------------------------------
Getter Method
Signature
ElementType
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX11.0.0.
License requirements: None.
SelectMesh¶
-
ThickenMeshBuilder.
SelectMesh
¶ Returns the select mesh
-------------------------------------
Getter Method
Signature
SelectMesh
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX11.0.0.
License requirements: None.
ThicknessValue¶
-
ThickenMeshBuilder.
ThicknessValue
¶ Returns the thickness value
-------------------------------------
Getter Method
Signature
ThicknessValue
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Method Detail¶
AutomaticThicknessValue¶
-
ThickenMeshBuilder.
AutomaticThicknessValue
¶ The creation of automatic thickness value
Signature
AutomaticThicknessValue()
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
ThickenMeshBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.