SweepBetweenMeshBuilder Class¶
-
class
NXOpen.CAE.
SweepBetweenMeshBuilder
¶ Bases:
NXOpen.Builder
Builder for creating swept mesh between faces.
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateSweepBetweenMeshBuilder()
New in version NX7.5.2.
Deprecated since version NX10.0.0: Use
CAE.Mesh3dHexBuilder
.
Properties¶
Property | Description |
---|---|
AutomaticSweepBetween | Returns the automatic sweep between mesh selection |
ElementType | Returns the element type builder. |
ManualSweepBetween | Returns the manual sweep between selection |
NumLayers | Returns or sets the number of layers |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of builder |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SweepBetweenMeshBuilderTypes Enumeration | creation type |
Property Detail¶
AutomaticSweepBetween¶
-
SweepBetweenMeshBuilder.
AutomaticSweepBetween
¶ Returns the automatic sweep between mesh selection
-------------------------------------
Getter Method
Signature
AutomaticSweepBetween
Returns: Return type: NXOpen.CAE.AutomaticSweepBetweenSelection
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElementType¶
-
SweepBetweenMeshBuilder.
ElementType
¶ Returns the element type builder.
-------------------------------------
Getter Method
Signature
ElementType
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
ManualSweepBetween¶
-
SweepBetweenMeshBuilder.
ManualSweepBetween
¶ Returns the manual sweep between selection
-------------------------------------
Getter Method
Signature
ManualSweepBetween
Returns: Return type: NXOpen.CAE.ManualSweepBetweenSelection
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
NumLayers¶
-
SweepBetweenMeshBuilder.
NumLayers
¶ Returns or sets the number of layers
-------------------------------------
Getter Method
Signature
NumLayers
Returns: Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
NumLayers
Parameters: numLayers (int) – New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
Type¶
-
SweepBetweenMeshBuilder.
Type
¶ Returns or sets the type of builder
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.CAE.SweepBetweenMeshBuilderTypes
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.CAE.SweepBetweenMeshBuilderTypes
) –New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
SweepBetweenMeshBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.