SurfaceCoatBuilder Class¶
-
class
NXOpen.CAE.
SurfaceCoatBuilder
¶ Bases:
NXOpen.Builder
Builder for creating Surface Coat
To create a new instance of this class, use
NXOpen.CAE.MeshManager.CreateSurfaceCoatBuilder()
New in version NX6.0.1.
Properties¶
Property | Description |
---|---|
ElementFace | Returns the selected element face(s) |
ElementType | Returns the element type to be created |
ExportToSolver | Returns or sets the export to solver toggle |
SelectGeometry | Returns the selected geometry object(s) |
SelectionMethodType | Returns or sets the selection method for different ways of selection |
SourceMesh | Returns the selected source object(s) |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitMesh | Commit the mesh |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SurfaceCoatBuilderSelectionMethod Enumeration | Represents the selection method to be used |
Property Detail¶
ElementFace¶
-
SurfaceCoatBuilder.
ElementFace
¶ Returns the selected element face(s)
-------------------------------------
Getter Method
Signature
ElementFace
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX6.0.1.
License requirements: None.
ElementType¶
-
SurfaceCoatBuilder.
ElementType
¶ Returns the element type to be created
-------------------------------------
Getter Method
Signature
ElementType
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX6.0.1.
License requirements: None.
ExportToSolver¶
-
SurfaceCoatBuilder.
ExportToSolver
¶ Returns or sets the export to solver toggle
-------------------------------------
Getter Method
Signature
ExportToSolver
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExportToSolver
Parameters: fExportToSolver (bool) – New in version NX7.5.0.
License requirements: None.
SelectGeometry¶
-
SurfaceCoatBuilder.
SelectGeometry
¶ Returns the selected geometry object(s)
-------------------------------------
Getter Method
Signature
SelectGeometry
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SelectionMethodType¶
-
SurfaceCoatBuilder.
SelectionMethodType
¶ Returns or sets the selection method for different ways of selection
-------------------------------------
Getter Method
Signature
SelectionMethodType
Returns: Return type: NXOpen.CAE.SurfaceCoatBuilderSelectionMethod
New in version NX6.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectionMethodType
Parameters: selectionMethodType ( NXOpen.CAE.SurfaceCoatBuilderSelectionMethod
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
SourceMesh¶
-
SurfaceCoatBuilder.
SourceMesh
¶ Returns the selected source object(s)
-------------------------------------
Getter Method
Signature
SourceMesh
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX6.0.1.
License requirements: None.
Method Detail¶
CommitMesh¶
-
SurfaceCoatBuilder.
CommitMesh
¶ Commit the mesh
Signature
CommitMesh()
Returns: Return type: NXOpen.CAE.Mesh
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
SurfaceCoatBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.