SpringEADBuilder Class¶
-
class
NXOpen.CAE.
SpringEADBuilder
¶ Bases:
NXOpen.Builder
This class provides Spring Associated Data Support
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateSpringEadBuilder()
Default values.
Property Value RotationalStiffness.Value 0 (millimeters part), 0 (inches part) StiffnessState Apply TranslationalStiffness.Value 0 (millimeters part), 0 (inches part) New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ComponentEndAState | Returns or sets the component end a state drives the action upon commit |
ComponentEndBState | Returns or sets the component end b state drives the action upon commit |
Elements | Returns the select element operator selects elements |
PhysicalPropertyTable | Returns or sets the physical property table of the spring element |
PhysicalPropertyTableState | Returns or sets the physical property table state state drives the action upon commit |
RotationalComponentEndA | Returns or sets the rotational component end A of the spring element |
RotationalComponentEndB | Returns or sets the rotational component end B of the spring element |
RotationalStiffness | Returns the expression rotational stiffness operator gets spring rotational stiffness value |
StiffnessState | Returns or sets the stiffness state drives the action upon commit |
Tag | Returns the Tag for this object. |
TranslationalComponentEndA | Returns or sets the translational component end A of the spring element |
TranslationalComponentEndB | Returns or sets the translational component end B of the spring element |
TranslationalStiffness | Returns the expression stiffness operator gets spring translational stiffness value |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SpringEADBuilderRotationalComponentEnd Enumeration | indicates which rotational degree of freedom to use as component end |
SpringEADBuilderState Enumeration | indicates to apply or clear the stiffness property upon commit |
SpringEADBuilderTranslationalComponentEnd Enumeration | indicates which translational degree of freedom to use as component end |
Property Detail¶
ComponentEndAState¶
-
SpringEADBuilder.
ComponentEndAState
¶ Returns or sets the component end a state drives the action upon commit
-------------------------------------
Getter Method
Signature
ComponentEndAState
Returns: Return type: NXOpen.CAE.SpringEADBuilderState
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
ComponentEndAState
Parameters: componentEndAState ( NXOpen.CAE.SpringEADBuilderState
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ComponentEndBState¶
-
SpringEADBuilder.
ComponentEndBState
¶ Returns or sets the component end b state drives the action upon commit
-------------------------------------
Getter Method
Signature
ComponentEndBState
Returns: Return type: NXOpen.CAE.SpringEADBuilderState
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
ComponentEndBState
Parameters: componentEndBState ( NXOpen.CAE.SpringEADBuilderState
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Elements¶
-
SpringEADBuilder.
Elements
¶ Returns the select element operator selects elements
-------------------------------------
Getter Method
Signature
Elements
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PhysicalPropertyTable¶
-
SpringEADBuilder.
PhysicalPropertyTable
¶ Returns or sets the physical property table of the spring element
-------------------------------------
Getter Method
Signature
PhysicalPropertyTable
Returns: Return type: NXOpen.CAE.PhysicalPropertyTable
New in version NX11.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
PhysicalPropertyTable
Parameters: physicalPropertyTable ( NXOpen.CAE.PhysicalPropertyTable
) –New in version NX11.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
PhysicalPropertyTableState¶
-
SpringEADBuilder.
PhysicalPropertyTableState
¶ Returns or sets the physical property table state state drives the action upon commit
-------------------------------------
Getter Method
Signature
PhysicalPropertyTableState
Returns: Return type: NXOpen.CAE.SpringEADBuilderState
New in version NX11.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
PhysicalPropertyTableState
Parameters: physicalPropertyTableState ( NXOpen.CAE.SpringEADBuilderState
) –New in version NX11.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
RotationalComponentEndA¶
-
SpringEADBuilder.
RotationalComponentEndA
¶ Returns or sets the rotational component end A of the spring element
-------------------------------------
Getter Method
Signature
RotationalComponentEndA
Returns: Return type: NXOpen.CAE.SpringEADBuilderRotationalComponentEnd
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
RotationalComponentEndA
Parameters: rotationalComponentEndA ( NXOpen.CAE.SpringEADBuilderRotationalComponentEnd
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
RotationalComponentEndB¶
-
SpringEADBuilder.
RotationalComponentEndB
¶ Returns or sets the rotational component end B of the spring element
-------------------------------------
Getter Method
Signature
RotationalComponentEndB
Returns: Return type: NXOpen.CAE.SpringEADBuilderRotationalComponentEnd
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
RotationalComponentEndB
Parameters: rotationalComponentEndB ( NXOpen.CAE.SpringEADBuilderRotationalComponentEnd
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
RotationalStiffness¶
-
SpringEADBuilder.
RotationalStiffness
¶ Returns the expression rotational stiffness operator gets spring rotational stiffness value
-------------------------------------
Getter Method
Signature
RotationalStiffness
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
StiffnessState¶
-
SpringEADBuilder.
StiffnessState
¶ Returns or sets the stiffness state drives the action upon commit
-------------------------------------
Getter Method
Signature
StiffnessState
Returns: Return type: NXOpen.CAE.SpringEADBuilderState
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
StiffnessState
Parameters: stiffnessState ( NXOpen.CAE.SpringEADBuilderState
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TranslationalComponentEndA¶
-
SpringEADBuilder.
TranslationalComponentEndA
¶ Returns or sets the translational component end A of the spring element
-------------------------------------
Getter Method
Signature
TranslationalComponentEndA
Returns: Return type: NXOpen.CAE.SpringEADBuilderTranslationalComponentEnd
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
TranslationalComponentEndA
Parameters: translationalComponentEndA ( NXOpen.CAE.SpringEADBuilderTranslationalComponentEnd
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TranslationalComponentEndB¶
-
SpringEADBuilder.
TranslationalComponentEndB
¶ Returns or sets the translational component end B of the spring element
-------------------------------------
Getter Method
Signature
TranslationalComponentEndB
Returns: Return type: NXOpen.CAE.SpringEADBuilderTranslationalComponentEnd
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
TranslationalComponentEndB
Parameters: translationalComponentEndB ( NXOpen.CAE.SpringEADBuilderTranslationalComponentEnd
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
TranslationalStiffness¶
-
SpringEADBuilder.
TranslationalStiffness
¶ Returns the expression stiffness operator gets spring translational stiffness value
-------------------------------------
Getter Method
Signature
TranslationalStiffness
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
SpringEADBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.