SpiderElementBuilder Class¶
-
class
NXOpen.CAE.
SpiderElementBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.SpiderElementBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateSpiderElementBuilder()
New in version NX5.0.1.
Properties¶
Property | Description |
---|---|
CollectorName | Returns or sets the mesh collector name |
CoreNode | Returns a core node |
Label | Returns or sets the label |
LegNodes | Returns the leg nodes |
MeshName | Returns or sets the mesh name |
NeutralName | Returns or sets the element neutral name |
NewMeshOption | Returns or sets the new mesh option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SpiderElementBuilderNewMeshType Enumeration | Option to create new mesh or add to existing mesh |
Property Detail¶
CollectorName¶
-
SpiderElementBuilder.
CollectorName
¶ Returns or sets the mesh collector name
-------------------------------------
Getter Method
Signature
CollectorName
Returns: Return type: str New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CollectorName
Parameters: collectorName (str) – New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
CoreNode¶
-
SpiderElementBuilder.
CoreNode
¶ Returns a core node
-------------------------------------
Getter Method
Signature
CoreNode
Returns: Return type: NXOpen.CAE.SelectFENode
New in version NX5.0.1.
License requirements: None.
Label¶
-
SpiderElementBuilder.
Label
¶ Returns or sets the label
-------------------------------------
Getter Method
Signature
Label
Returns: Return type: int New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label
Parameters: label (int) – New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
LegNodes¶
-
SpiderElementBuilder.
LegNodes
¶ Returns the leg nodes
-------------------------------------
Getter Method
Signature
LegNodes
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX5.0.1.
License requirements: None.
MeshName¶
-
SpiderElementBuilder.
MeshName
¶ Returns or sets the mesh name
-------------------------------------
Getter Method
Signature
MeshName
Returns: Return type: str New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeshName
Parameters: meshName (str) – New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
NeutralName¶
-
SpiderElementBuilder.
NeutralName
¶ Returns or sets the element neutral name
-------------------------------------
Getter Method
Signature
NeutralName
Returns: Return type: str New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
NeutralName
Parameters: neutralName (str) – New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
NewMeshOption¶
-
SpiderElementBuilder.
NewMeshOption
¶ Returns or sets the new mesh option
-------------------------------------
Getter Method
Signature
NewMeshOption
Returns: Return type: NXOpen.CAE.SpiderElementBuilderNewMeshType
New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewMeshOption
Parameters: newMeshOption ( NXOpen.CAE.SpiderElementBuilderNewMeshType
) –New in version NX5.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
SpiderElementBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.