SolutionManager Class¶
-
class
NXOpen.CAE.
SolutionManager
¶ Bases:
NXOpen.CAE.LbcAssociationMgr
Represents
NXOpen.CAE.SolutionManager
To create a new instance of this class, use
NXOpen.CAE.SimSimulation.CreateSolutionManager()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Orientation | Returns or sets the export orientation option |
Tag | Returns the Tag for this object. |
TypeOption | Returns or sets the bc type option |
Methods¶
Method | Description |
---|---|
AddBc | Add bc to a solution |
AddFolder | Add bc folder to a solution |
AddLoadset | Add loadset to a solution |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ExportToCsv | Export to csv |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ImportFromCsv | Import from csv |
RemoveBc | Remove bc from a solution |
RemoveFolder | Remove bc folder from a solution |
RemoveLoadset | Remove loadset from a solution |
ScaleBc | Set scale factor on bc in a solution |
ScaleFolder | Set scale factor on bc folder in a solution |
ScaleLoadset | Set scale factor on loadset in a solution |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
AddBc¶
-
SolutionManager.
AddBc
¶ Add bc to a solution
Signature
AddBc(tSolution, tBc)
Parameters: - tSolution (
NXOpen.CAE.SimSolution
) – solution - tBc (
NXOpen.CAE.SimBC
) – bc object
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- tSolution (
AddFolder¶
-
SolutionManager.
AddFolder
¶ Add bc folder to a solution
Signature
AddFolder(tSolution, tBc)
Parameters: - tSolution (
NXOpen.CAE.SimSolution
) – solution - tBc (
NXOpen.CAE.SimLbcFolder
) – bc folder object
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- tSolution (
AddLoadset¶
-
SolutionManager.
AddLoadset
¶ Add loadset to a solution
Signature
AddLoadset(tSolution, tBc)
Parameters: - tSolution (
NXOpen.CAE.SimSolution
) – solution - tBc (
NXOpen.CAE.SimLoadSet
) – loadset object
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- tSolution (
RemoveBc¶
-
SolutionManager.
RemoveBc
¶ Remove bc from a solution
Signature
RemoveBc(tSolution, tBc)
Parameters: - tSolution (
NXOpen.CAE.SimSolution
) – solution - tBc (
NXOpen.CAE.SimBC
) – bc object
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- tSolution (
RemoveFolder¶
-
SolutionManager.
RemoveFolder
¶ Remove bc folder from a solution
Signature
RemoveFolder(tSolution, tBc)
Parameters: - tSolution (
NXOpen.CAE.SimSolution
) – solution - tBc (
NXOpen.CAE.SimLbcFolder
) – bc folder object
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- tSolution (
RemoveLoadset¶
-
SolutionManager.
RemoveLoadset
¶ Remove loadset from a solution
Signature
RemoveLoadset(tSolution, tBc)
Parameters: - tSolution (
NXOpen.CAE.SimSolution
) – solution - tBc (
NXOpen.CAE.SimLoadSet
) – loadset object
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- tSolution (
ScaleBc¶
-
SolutionManager.
ScaleBc
¶ Set scale factor on bc in a solution
Signature
ScaleBc(tSolution, tBc, scale)
Parameters: - tSolution (
NXOpen.CAE.SimSolution
) – solution - tBc (
NXOpen.CAE.SimBC
) – bc object - scale (float) – scale factor
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- tSolution (
ScaleFolder¶
-
SolutionManager.
ScaleFolder
¶ Set scale factor on bc folder in a solution
Signature
ScaleFolder(tSolution, tBc, scale)
Parameters: - tSolution (
NXOpen.CAE.SimSolution
) – solution - tBc (
NXOpen.CAE.SimLbcFolder
) – bc folder object - scale (float) – scale factor
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- tSolution (
ScaleLoadset¶
-
SolutionManager.
ScaleLoadset
¶ Set scale factor on loadset in a solution
Signature
ScaleLoadset(tSolution, tBc, scale)
Parameters: - tSolution (
NXOpen.CAE.SimSolution
) – solution - tBc (
NXOpen.CAE.SimLoadSet
) – loadset object - scale (float) – scale factor
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- tSolution (
Validate¶
-
SolutionManager.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.