SolidPropertyCheckBuilderUserUnit Enumeration¶
NXOpen.CAE.SolidPropertyCheckBuilder.UserUnit is an alias for NXOpen.CAE.SolidPropertyCheckBuilderUserUnit
-
class
NXOpen.CAE.
SolidPropertyCheckBuilderUserUnit
¶ Bases:
object
User Specified output unit
Enum Members
Enum Member Enum Member Description DefaultUnit Load unit = same as system default unit KgMilli mass = kg, cg = mm, volume = mm^3 mmoi = kg-mm^2 LbmIn mass = lbm, cg = in, volume = in^3 mmoi = lbm-in^2 LbfInSec mass = lbf-sec^2/in, cg = in, volume = in^3 mmoi = lbf-in-sec^2 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-