SketchCurvesCollection Class

class NXOpen.CAE.SketchCurvesCollection

Bases: object

Represents the collection of all NXOpen.CAE.SketchCurves in a fem part

To obtain an instance of this class, refer to NXOpen.CAE.BaseFemPart

New in version NX7.5.0.

Methods

Method Description
FindObject Finds the NXOpen.CAE.SketchCurves with the given identifier as recorded in a journal.

Method Detail

FindObject

SketchCurvesCollection.FindObject

Finds the NXOpen.CAE.SketchCurves with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object can be found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Sketch Curves name
Returns:Sketch Curves with this identifier
Return type:NXOpen.CAE.SketchCurves

New in version NX5.0.0.

License requirements: None.