SimLoadSetCollection Class¶
-
class
NXOpen.CAE.
SimLoadSetCollection
¶ Bases:
object
Provides methods for managing
NXOpen.CAE.SimLoadSet
in a sim partTo obtain an instance of this class, refer to
NXOpen.CAE.SimSimulation
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateLoadSet | Creates a NXOpen.CAE.SimLoadSet |
FindObject | Finds the NXOpen.CAE.SimLoadSet with the given identifier as recorded in a journal. |
Method Detail¶
CreateLoadSet¶
-
SimLoadSetCollection.
CreateLoadSet
¶ Creates a
NXOpen.CAE.SimLoadSet
Signature
CreateLoadSet(descriptorName, name, label)
Parameters: - descriptorName (str) – Name of the load set descriptor
- name (str) – Name of the load set
- label (int) – Label of the load set, input 0 to get next available label
Returns: Load set object created
Return type: New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
SimLoadSetCollection.
FindObject
¶ Finds the
NXOpen.CAE.SimLoadSet
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Load set found Return type: NXOpen.CAE.SimLoadSet
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)