SimLoadRecipeTypesDataTypes Enumeration¶
NXOpen.CAE.SimLoadRecipeTypes.DataTypes is an alias for NXOpen.CAE.SimLoadRecipeTypesDataTypes
-
class
NXOpen.CAE.
SimLoadRecipeTypesDataTypes
¶ Bases:
object
This enum defines the Data Type options
Enum Members
Enum Member Enum Member Description TimeData Time Data FrequencySpectra Frequency Spectra WaterfallofTimeData Waterfall of Time Data WaterfallofFrequencySpectra Waterfall of Frequency Spectra OrderCut Order Cut -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-