SimLoadRecipeMapEntryTargetTypesTargetTypes Enumeration¶
NXOpen.CAE.SimLoadRecipeMapEntryTargetTypes.TargetTypes is an alias for NXOpen.CAE.SimLoadRecipeMapEntryTargetTypesTargetTypes
-
class
NXOpen.CAE.
SimLoadRecipeMapEntryTargetTypesTargetTypes
¶ Bases:
object
This enum defines the target type options of a
NXOpen.CAE.SimLoadRecipeMapEntry
Enum Members
Enum Member Enum Member Description Unknown Unkown target type Node Node NodeGroup Nodes in a group. NodeMesh Nodes in a mesh. Face Element face FaceGroup Element faces in a group. FaceMesh Element faces in a mesh. NodeFem Nodes in a fem model. FaceFem Element faces in a fem model. NodeSelectionRecipe Nodes in the contents of a CAE.SelectionRecipe
FaceSelectionRecipe Element faces in the contents of a CAE.SelectionRecipe
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-