SimConstraintSetCollection Class¶
-
class
NXOpen.CAE.
SimConstraintSetCollection
¶ Bases:
object
Provides methods for managing
SimConstraintSet
in a sim partTo obtain an instance of this class, refer to
NXOpen.CAE.SimSimulation
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateConstraintSet | Creates a NXOpen.CAE.SimConstraintSet |
FindObject | Finds the NXOpen.CAE.SimConstraintSet with the given identifier as recorded in a journal. |
Method Detail¶
CreateConstraintSet¶
-
SimConstraintSetCollection.
CreateConstraintSet
¶ Creates a
NXOpen.CAE.SimConstraintSet
Signature
CreateConstraintSet(descriptorName, name, label)
Parameters: - descriptorName (str) – Name of the constraint set descriptor
- name (str) – Name of the constraint set
- label (int) – Label of the constraint set, input 0 to get next available label
Returns: Constraint set object created
Return type: New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
SimConstraintSetCollection.
FindObject
¶ Finds the
NXOpen.CAE.SimConstraintSet
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Constraint set found Return type: NXOpen.CAE.SimConstraintSet
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)