SimConditionTimeStep Class¶
-
class
NXOpen.CAE.
SimConditionTimeStep
¶ Bases:
NXOpen.TaggedObject
This class represents a step in the time history of a
NXOpen.CAE.SimConditionSequence
. The time history of aNXOpen.CAE.SimConditionSequence
is a time ordered list ofNXOpen.CAE.SimConditionTimeStep
.An instance of this class can be obtained from
NXOpen.CAE.SimConditionSequence
.New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Condition | Returns or sets the Time Step condition |
Description | Returns or sets the Time Step description |
Tag | Returns the Tag for this object. |
Time | Returns the Time Step time |
Methods¶
Property Detail¶
Condition¶
-
SimConditionTimeStep.
Condition
¶ Returns or sets the Time Step condition
-------------------------------------
Getter Method
Signature
Condition
Returns: the NXOpen.CAE.SimCondition
ObjectReturn type: NXOpen.CAE.SimCondition
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Condition
Parameters: condition ( NXOpen.CAE.SimCondition
) –New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Description¶
-
SimConditionTimeStep.
Description
¶ Returns or sets the Time Step description
-------------------------------------
Getter Method
Signature
Description
Returns: the description value Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Description
Parameters: description (str) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)