SimConditionSequenceCollection Class¶
-
class
NXOpen.CAE.
SimConditionSequenceCollection
¶ Bases:
object
This class is a collection of
NXOpen.CAE.SimConditionSequence
. For now, it only supports oneNXOpen.CAE.SimConditionSequence
. To access the one and onlyNXOpen.CAE.SimConditionSequence
, useNXOpen.CAE.SimConditionSeqMgr.ActiveConditionSequence`()
To obtain an instance of this class, refer to
NXOpen.CAE.SimConditionSeqMgr
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
Find | Collection’s object finder |
Get | Returns the NXOpen.CAE.SimConditionSequence with the specified label or None if such a sequence doesn’t exist |
Method Detail¶
Find¶
-
SimConditionSequenceCollection.
Find
¶ Collection’s object finder
Signature
Find(label)
Parameters: label (str) – label of the NXOpen.CAE.SimConditionSequence
Returns: The NXOpen.CAE.SimConditionSequence
Return type: NXOpen.CAE.SimConditionSequence
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Get¶
-
SimConditionSequenceCollection.
Get
¶ Returns the
NXOpen.CAE.SimConditionSequence
with the specified label or None if such a sequence doesn’t existSignature
Get(label)
Parameters: label (int) – Returns: the corresponding NXOpen.CAE.SimConditionSequence
Return type: NXOpen.CAE.SimConditionSequence
New in version NX9.0.0.
License requirements: None.