SimConditionSeqMgrFileFormat Enumeration

NXOpen.CAE.SimConditionSeqMgr.FileFormat is an alias for NXOpen.CAE.SimConditionSeqMgrFileFormat

class NXOpen.CAE.SimConditionSeqMgrFileFormat

Bases: object

Specifies the file format during an import.

Enum Members

Enum Member Enum Member Description
Bdd
Xml
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.