SimBcXyPlotBuilderResolveMultipleMatches Enumeration

NXOpen.CAE.SimBcXyPlotBuilder.ResolveMultipleMatches is an alias for NXOpen.CAE.SimBcXyPlotBuilderResolveMultipleMatches

class NXOpen.CAE.SimBcXyPlotBuilderResolveMultipleMatches

Bases: object

Resolve multiple matches when the location specified matches multiple items in the boundary condition’s target set

Enum Members

Enum Member Enum Member Description
Add
Average
Minimum
Maximum
MultipleCurves
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.