SimBcPlotContoursBuilderResolveOverlapType Enumeration

NXOpen.CAE.SimBcPlotContoursBuilder.ResolveOverlapType is an alias for NXOpen.CAE.SimBcPlotContoursBuilderResolveOverlapType

class NXOpen.CAE.SimBcPlotContoursBuilderResolveOverlapType

Bases: object

Resolve overlap types

Enum Members

Enum Member Enum Member Description
Add
Average
Maximum
Minimum
Specify
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.