SimBCDisplayMode Enumeration¶
NXOpen.CAE.SimBCDisplay.Mode is an alias for NXOpen.CAE.SimBCDisplayMode
-
class
NXOpen.CAE.
SimBCDisplayMode
¶ Bases:
object
Used to specify the display mode for the BC
Enum Members
Enum Member Enum Member Description Collapse Set a collapsed display mode Expand Set an expanded display mode Offset Set an offset display mode. Draw the edge BC display using an offset line along the BC target locations -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-