SignalProcessingDBSettings Class¶
-
class
NXOpen.CAE.
SignalProcessingDBSettings
¶ Bases:
NXOpen.TaggedObject
This is the class handling the dB settings option: a dB reference value and a dB format (10 or 20).
This object is initialized with a Part::Unit::Type. Based on the measure type of this unit, a default dB reference value is retrieved from the customer defaults and a dB format is applied.
In addition, for measure types which are defined in the customer defaults, a MKS unit is derived, in which the dB reference is expressed. The GetConvertedReference method returns the dB reference value converted to the unit that was specified when constructing the object.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
DBFormat | Returns or sets the dB format to apply |
DBReference | Returns or sets the dB reference to apply |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetReferenceForTargetUnit | Gets the dB reference value converted to the units of the data. |
Enumerations¶
SignalProcessingDBSettingsDBFormats Enumeration | This enum defines the dB formats |
Property Detail¶
DBFormat¶
-
SignalProcessingDBSettings.
DBFormat
¶ Returns or sets the dB format to apply
-------------------------------------
Getter Method
Signature
DBFormat
Returns: Return type: NXOpen.CAE.SignalProcessingDBSettingsDBFormats
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DBFormat
Parameters: format ( NXOpen.CAE.SignalProcessingDBSettingsDBFormats
) –New in version NX12.0.0.
License requirements: None.
DBReference¶
-
SignalProcessingDBSettings.
DBReference
¶ Returns or sets the dB reference to apply
-------------------------------------
Getter Method
Signature
DBReference
Returns: Return type: float New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DBReference
Parameters: dBReference (float) – New in version NX12.0.0.
License requirements: None.
Method Detail¶
GetReferenceForTargetUnit¶
-
SignalProcessingDBSettings.
GetReferenceForTargetUnit
¶ Gets the dB reference value converted to the units of the data.
Signature
GetReferenceForTargetUnit(targetUnit)
Parameters: targetUnit ( NXOpen.Unit
) –Returns: Return type: float New in version NX12.0.0.
License requirements: None.