ShowHideManager Class¶
-
class
NXOpen.CAE.
ShowHideManager
¶ Bases:
object
Provides method for creating builder for Show Hide operation commands in a fem/sim part
To obtain an instance of this class, refer to
NXOpen.CAE.CaePart
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateShowAdjacentBuilder | Creates a builder for Show Adjacent Command |
CreateShowHideBuilder | Creates a builder for Show Hide Command |
CreateShowOnlyBuilder | Creates a builder for Show Only Command |
ReverseFaceDisplay | Creates a builder for the Reverse Face Display Command, which reverses the display of each CAE geometry face in the model. |
Method Detail¶
CreateShowAdjacentBuilder¶
-
ShowHideManager.
CreateShowAdjacentBuilder
¶ Creates a builder for Show Adjacent Command
Signature
CreateShowAdjacentBuilder()
Returns: Return type: NXOpen.CAE.ShowAdjacentBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateShowHideBuilder¶
-
ShowHideManager.
CreateShowHideBuilder
¶ Creates a builder for Show Hide Command
Signature
CreateShowHideBuilder()
Returns: Return type: NXOpen.CAE.ShowHideBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateShowOnlyBuilder¶
-
ShowHideManager.
CreateShowOnlyBuilder
¶ Creates a builder for Show Only Command
Signature
CreateShowOnlyBuilder()
Returns: Return type: NXOpen.CAE.ShowOnlyBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ReverseFaceDisplay¶
-
ShowHideManager.
ReverseFaceDisplay
¶ Creates a builder for the Reverse Face Display Command, which reverses the display of each CAE geometry face in the model.
Use this method associated with
NXOpen.CAE.ShowHideManager.CreateShowOnlyBuilder()
to examine the CAE model visually. For example, use the show only to visually check the a BC’s target sets, and then use reverse face display to visually examine the CAE geometry which doesn’t have this BC defined on it.Signature
ReverseFaceDisplay()
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)