ShipMeshAutomationBuilder Class¶
-
class
NXOpen.CAE.
ShipMeshAutomationBuilder
¶ Bases:
NXOpen.Builder
Represents Ship Mesh Automation * Used to create a
NXOpen.CAE.ShipMeshAutomation
To create a new instance of this class, use
NXOpen.CAE.MeshManager.CreateShipMeshAutomationBuilder()
New in version NX11.0.2.
Properties¶
Property | Description |
---|---|
DefaultElementSize | Returns or sets the flag to indicate whether to use the default mesh element size which is evaluated automatically |
ElementSize | Returns the value of meshing element size |
MethodType | Returns or sets the method type of creating mesh elements |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ShipMeshAutomationBuilderMeshingMethodType Enumeration | the meshing method type |
Property Detail¶
DefaultElementSize¶
-
ShipMeshAutomationBuilder.
DefaultElementSize
¶ Returns or sets the flag to indicate whether to use the default mesh element size which is evaluated automatically
-------------------------------------
Getter Method
Signature
DefaultElementSize
Returns: Return type: bool New in version NX11.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”), nx_ship_basic (“Ship Basic Design”)
-------------------------------------
Setter Method
Signature
DefaultElementSize
Parameters: fDefaultElementSize (bool) – New in version NX11.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”), nx_ship_basic (“Ship Basic Design”)
ElementSize¶
-
ShipMeshAutomationBuilder.
ElementSize
¶ Returns the value of meshing element size
-------------------------------------
Getter Method
Signature
ElementSize
Returns: Return type: NXOpen.Expression
New in version NX11.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”), nx_ship_basic (“Ship Basic Design”)
MethodType¶
-
ShipMeshAutomationBuilder.
MethodType
¶ Returns or sets the method type of creating mesh elements
-------------------------------------
Getter Method
Signature
MethodType
Returns: Return type: NXOpen.CAE.ShipMeshAutomationBuilderMeshingMethodType
New in version NX11.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”), nx_ship_basic (“Ship Basic Design”)
-------------------------------------
Setter Method
Signature
MethodType
Parameters: methodType ( NXOpen.CAE.ShipMeshAutomationBuilderMeshingMethodType
) –New in version NX11.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”), nx_ship_basic (“Ship Basic Design”)
Method Detail¶
Validate¶
-
ShipMeshAutomationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.