ShellEADBuilder Class¶
-
class
NXOpen.CAE.
ShellEADBuilder
¶ Bases:
NXOpen.Builder
This class provides Shell Associated Data Support
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateShellEadBuilder()
Default values.
Property Value GapThicknessState Ignore MaterialOrientationState Ignore PhysicalPropertyTableState Ignore SetMatOriMethod CoordinateSystem ThicknessState Ignore ZoffsetState Ignore New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CoordinateSystem | Returns or sets the get coordinate system method gets the coordinate system for orienting by coordinate system |
CsysDataType | Returns or sets the get selection csys data type gets coordinate system data type |
Elements | Returns the select element operator selects elements |
GapThicknessExpression | Returns the gap thickness expression of the shell element |
GapThicknessState | Returns or sets the gap thickness state drives the action upon commit |
MaterialOrientationState | Returns or sets the material orientation state drives the action upon commit |
Node | Returns the select nodes operator selects nodes to limit thickness to |
NodeGaps | Returns the select nodes operator selects nodes to limit gap thickness to |
PhysicalPropertyTable | Returns or sets the physical property table of the shell element |
PhysicalPropertyTableState | Returns or sets the physical property table state state drives the action upon commit |
PointInPlane | Returns or sets the get coordinate system data point in plane gets the coordinates of point in x-z plane if cartesian csys or point in azimuthal origin plane if cylindrical/ spherical csys for material orientation |
PointOnZaxis | Returns or sets the get coordinate system data point on z axis gets the coordinates of point on z-axis for material orientation |
PointOrigin | Returns or sets the get coordinate system data point origin gets the coordinates of origin point for material orientation |
PreferredLabel | Returns or sets the get preferred csys label gets the label assigned to the csys data |
SetMatOriMethod | Returns or sets the get selection ori operator gets material orientation method |
Tag | Returns the Tag for this object. |
ThicknessExpression | Returns the thickness expression of the shell element |
ThicknessState | Returns or sets the thickness state drives the action upon commit |
Vector | Returns or sets the get vector method gets the projection vector for material orientation |
ZoffsetExpression | Returns the zoffset expression of the shell element |
ZoffsetState | Returns or sets the zoffset state drives the action upon commit |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ShellEADBuilderCoordinateSystemDataType Enumeration | indicates which type of coordinate system data to use |
ShellEADBuilderMaterialOrientationMethod Enumeration | indicates which material orientation method to use |
ShellEADBuilderState Enumeration | indicates to ignore, apply or clear the state property upon commit |
Property Detail¶
CoordinateSystem¶
-
ShellEADBuilder.
CoordinateSystem
¶ Returns or sets the get coordinate system method gets the coordinate system for orienting by coordinate system
-------------------------------------
Getter Method
Signature
CoordinateSystem
Returns: Return type: NXOpen.CoordinateSystem
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
CoordinateSystem
Parameters: coordinateSystem ( NXOpen.CoordinateSystem
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CsysDataType¶
-
ShellEADBuilder.
CsysDataType
¶ Returns or sets the get selection csys data type gets coordinate system data type
-------------------------------------
Getter Method
Signature
CsysDataType
Returns: Return type: NXOpen.CAE.ShellEADBuilderCoordinateSystemDataType
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
CsysDataType
Parameters: csysDataType ( NXOpen.CAE.ShellEADBuilderCoordinateSystemDataType
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Elements¶
-
ShellEADBuilder.
Elements
¶ Returns the select element operator selects elements
-------------------------------------
Getter Method
Signature
Elements
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GapThicknessExpression¶
-
ShellEADBuilder.
GapThicknessExpression
¶ Returns the gap thickness expression of the shell element
-------------------------------------
Getter Method
Signature
GapThicknessExpression
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GapThicknessState¶
-
ShellEADBuilder.
GapThicknessState
¶ Returns or sets the gap thickness state drives the action upon commit
-------------------------------------
Getter Method
Signature
GapThicknessState
Returns: Return type: NXOpen.CAE.ShellEADBuilderState
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
GapThicknessState
Parameters: gapThicknessState ( NXOpen.CAE.ShellEADBuilderState
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MaterialOrientationState¶
-
ShellEADBuilder.
MaterialOrientationState
¶ Returns or sets the material orientation state drives the action upon commit
-------------------------------------
Getter Method
Signature
MaterialOrientationState
Returns: Return type: NXOpen.CAE.ShellEADBuilderState
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
MaterialOrientationState
Parameters: materialOrientationState ( NXOpen.CAE.ShellEADBuilderState
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Node¶
-
ShellEADBuilder.
Node
¶ Returns the select nodes operator selects nodes to limit thickness to
-------------------------------------
Getter Method
Signature
Node
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
NodeGaps¶
-
ShellEADBuilder.
NodeGaps
¶ Returns the select nodes operator selects nodes to limit gap thickness to
-------------------------------------
Getter Method
Signature
NodeGaps
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PhysicalPropertyTable¶
-
ShellEADBuilder.
PhysicalPropertyTable
¶ Returns or sets the physical property table of the shell element
-------------------------------------
Getter Method
Signature
PhysicalPropertyTable
Returns: Return type: NXOpen.CAE.PhysicalPropertyTable
New in version NX11.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
PhysicalPropertyTable
Parameters: physicalPropertyTable ( NXOpen.CAE.PhysicalPropertyTable
) –New in version NX11.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
PhysicalPropertyTableState¶
-
ShellEADBuilder.
PhysicalPropertyTableState
¶ Returns or sets the physical property table state state drives the action upon commit
-------------------------------------
Getter Method
Signature
PhysicalPropertyTableState
Returns: Return type: NXOpen.CAE.ShellEADBuilderState
New in version NX11.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
PhysicalPropertyTableState
Parameters: physicalPropertyTableState ( NXOpen.CAE.ShellEADBuilderState
) –New in version NX11.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
PointInPlane¶
-
ShellEADBuilder.
PointInPlane
¶ Returns or sets the get coordinate system data point in plane gets the coordinates of point in x-z plane if cartesian csys or point in azimuthal origin plane if cylindrical/ spherical csys for material orientation
-------------------------------------
Getter Method
Signature
PointInPlane
Returns: material orientation csys data point in the x-z plane if cartesian csys or azimuthal origin plane if cylindrical/spherical csys Return type: NXOpen.Point
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
PointInPlane
Parameters: planePoint ( NXOpen.Point
) – material orientation csys data point in the x-z plane if cartesian csys or azimuthal origin plane if cylindrical/spherical csysNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PointOnZaxis¶
-
ShellEADBuilder.
PointOnZaxis
¶ Returns or sets the get coordinate system data point on z axis gets the coordinates of point on z-axis for material orientation
-------------------------------------
Getter Method
Signature
PointOnZaxis
Returns: material orientation csys data point on z-axis Return type: NXOpen.Point
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
PointOnZaxis
Parameters: zAxisPoint ( NXOpen.Point
) – material orientation csys data point on z-axisNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PointOrigin¶
-
ShellEADBuilder.
PointOrigin
¶ Returns or sets the get coordinate system data point origin gets the coordinates of origin point for material orientation
-------------------------------------
Getter Method
Signature
PointOrigin
Returns: material orientation csys data origin point Return type: NXOpen.Point
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
PointOrigin
Parameters: originPoint ( NXOpen.Point
) – material orientation csys data origin pointNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PreferredLabel¶
-
ShellEADBuilder.
PreferredLabel
¶ Returns or sets the get preferred csys label gets the label assigned to the csys data
-------------------------------------
Getter Method
Signature
PreferredLabel
Returns: Return type: int New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
PreferredLabel
Parameters: preferredLabel (int) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetMatOriMethod¶
-
ShellEADBuilder.
SetMatOriMethod
¶ Returns or sets the get selection ori operator gets material orientation method
-------------------------------------
Getter Method
Signature
SetMatOriMethod
Returns: Return type: NXOpen.CAE.ShellEADBuilderMaterialOrientationMethod
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
SetMatOriMethod
Parameters: setMatOriMethod ( NXOpen.CAE.ShellEADBuilderMaterialOrientationMethod
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ThicknessExpression¶
-
ShellEADBuilder.
ThicknessExpression
¶ Returns the thickness expression of the shell element
-------------------------------------
Getter Method
Signature
ThicknessExpression
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ThicknessState¶
-
ShellEADBuilder.
ThicknessState
¶ Returns or sets the thickness state drives the action upon commit
-------------------------------------
Getter Method
Signature
ThicknessState
Returns: Return type: NXOpen.CAE.ShellEADBuilderState
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
ThicknessState
Parameters: thicknessState ( NXOpen.CAE.ShellEADBuilderState
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Vector¶
-
ShellEADBuilder.
Vector
¶ Returns or sets the get vector method gets the projection vector for material orientation
-------------------------------------
Getter Method
Signature
Vector
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
Vector
Parameters: vector ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ZoffsetExpression¶
-
ShellEADBuilder.
ZoffsetExpression
¶ Returns the zoffset expression of the shell element
-------------------------------------
Getter Method
Signature
ZoffsetExpression
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ZoffsetState¶
-
ShellEADBuilder.
ZoffsetState
¶ Returns or sets the zoffset state drives the action upon commit
-------------------------------------
Getter Method
Signature
ZoffsetState
Returns: Return type: NXOpen.CAE.ShellEADBuilderState
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
ZoffsetState
Parameters: zoffsetState ( NXOpen.CAE.ShellEADBuilderState
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
ShellEADBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.