RigidEADBuilder Class¶
-
class
NXOpen.CAE.
RigidEADBuilder
¶ Bases:
NXOpen.Builder
This class provides Rigid Associated Data Support
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateRigidEadBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DofsState | Returns or sets the dofs state drives the action upon commit |
Elements | Returns the select element operator selects elements |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDofs | The set operator for the 6 dofs of the rigid element |
GetObject | Returns the object currently being edited by this builder. |
SetDofs | The get operator for the 6 dofs of the rigid element |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RigidEADBuilderDof Enumeration | indicates if a dof is on or off |
RigidEADBuilderState Enumeration | indicates to apply or clear the stiffness property upon commit |
Property Detail¶
DofsState¶
-
RigidEADBuilder.
DofsState
¶ Returns or sets the dofs state drives the action upon commit
-------------------------------------
Getter Method
Signature
DofsState
Returns: Return type: NXOpen.CAE.RigidEADBuilderState
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
DofsState
Parameters: dofsState ( NXOpen.CAE.RigidEADBuilderState
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Elements¶
-
RigidEADBuilder.
Elements
¶ Returns the select element operator selects elements
-------------------------------------
Getter Method
Signature
Elements
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
GetDofs¶
-
RigidEADBuilder.
GetDofs
¶ The set operator for the 6 dofs of the rigid element
Signature
GetDofs()
Returns: Return type: list of NXOpen.CAE.RigidEADBuilderDof
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetDofs¶
-
RigidEADBuilder.
SetDofs
¶ The get operator for the 6 dofs of the rigid element
Signature
SetDofs(dofs)
Parameters: dofs (list of NXOpen.CAE.RigidEADBuilderDof
) –New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
RigidEADBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.