ResultsReductionBuilderOutput Enumeration

NXOpen.CAE.ResultsReductionBuilder.Output is an alias for NXOpen.CAE.ResultsReductionBuilderOutput

class NXOpen.CAE.ResultsReductionBuilderOutput

Bases: object

output types

Enum Members

Enum Member Enum Member Description
ExportResultFile
CreatePostView
CreateField
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.