ResultsReductionBuilderIncompatibleResults Enumeration

NXOpen.CAE.ResultsReductionBuilder.IncompatibleResults is an alias for NXOpen.CAE.ResultsReductionBuilderIncompatibleResults

class NXOpen.CAE.ResultsReductionBuilderIncompatibleResults

Bases: object

Incompatible results options

Enum Members

Enum Member Enum Member Description
Skip
Abort
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.