ResultsManipulationBuilderResultAppendMethod Enumeration

NXOpen.CAE.ResultsManipulationBuilder.ResultAppendMethod is an alias for NXOpen.CAE.ResultsManipulationBuilderResultAppendMethod

class NXOpen.CAE.ResultsManipulationBuilderResultAppendMethod

Bases: object

Result Append Method options

Enum Members

Enum Member Enum Member Description
CreateNewLoadCases
MergeWithPrimaryResultsData
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.