ResultsManipulationBuilderOutputResultType Enumeration

NXOpen.CAE.ResultsManipulationBuilder.OutputResultType is an alias for NXOpen.CAE.ResultsManipulationBuilderOutputResultType

class NXOpen.CAE.ResultsManipulationBuilderOutputResultType

Bases: object

Output result types

Enum Members

Enum Member Enum Member Description
Companion
Full
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.