ResultsManipulationBuilderElementValueAtNode Enumeration

NXOpen.CAE.ResultsManipulationBuilder.ElementValueAtNode is an alias for NXOpen.CAE.ResultsManipulationBuilderElementValueAtNode

class NXOpen.CAE.ResultsManipulationBuilderElementValueAtNode

Bases: object

Value at Nodes for element nodal values

Enum Members

Enum Member Enum Member Description
Average
Maximum
Minimum
Sum
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.