ResultsCombinationBuilderEvaluationError Enumeration

NXOpen.CAE.ResultsCombinationBuilder.EvaluationError is an alias for NXOpen.CAE.ResultsCombinationBuilderEvaluationError

class NXOpen.CAE.ResultsCombinationBuilderEvaluationError

Bases: object

evaluation error options

Enum Members

Enum Member Enum Member Description
Skip
ZeroFill
Abort
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.