ResultProbeBuilderNodalCombination Enumeration

NXOpen.CAE.ResultProbeBuilder.NodalCombination is an alias for NXOpen.CAE.ResultProbeBuilderNodalCombination

class NXOpen.CAE.ResultProbeBuilderNodalCombination

Bases: object

Options to combine multiple geometry values

Enum Members

Enum Member Enum Member Description
ArithmeticMean
Minimum
Maximum
Sum
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.