ResultLoadcaseValueType Enumeration

NXOpen.CAE.Result.LoadcaseValueType is an alias for NXOpen.CAE.ResultLoadcaseValueType

class NXOpen.CAE.ResultLoadcaseValueType

Bases: object

Value type for result load case

Enum Members

Enum Member Enum Member Description
Unknown Unknown Value type
Frequency Value type - Frequency
LoadFactor Value type - Load Factor
NodeDOF Value type - Node DOF
LoadCase Value type - Load Case
Time Value type - Time
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.