ResultInitialDeformationSelection Enumeration¶
NXOpen.CAE.Result.InitialDeformationSelection is an alias for NXOpen.CAE.ResultInitialDeformationSelection
-
class
NXOpen.CAE.
ResultInitialDeformationSelection
¶ Bases:
object
The initial deformation selection type which will decide how the final calculations will happen after applying the initial deformation on the main deforamtion.
Enum Members
Enum Member Enum Member Description NotSet None Default Default selection UserDefined Selection from the user -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-