ResultCoordinateSystemSource Enumeration¶
NXOpen.CAE.Result.CoordinateSystemSource is an alias for NXOpen.CAE.ResultCoordinateSystemSource
-
class
NXOpen.CAE.
ResultCoordinateSystemSource
¶ Bases:
object
Source of selected coordinate system
Enum Members
Enum Member Enum Member Description NotSet Model identifies a coordinate system in the work part Result identifies a coordinate system in the result -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-