ResultComputationType Enumeration¶
NXOpen.CAE.Result.ComputationType is an alias for NXOpen.CAE.ResultComputationType
-
class
NXOpen.CAE.
ResultComputationType
¶ Bases:
object
types for different way of computing nodal result from element nodal result.
Enum Members
Enum Member Enum Member Description NotSet None Average compute average Sum compute sum. (Applicable only for element-nodal vector result.) Minimum minimum value at the node Maximum maximum value at the node AbsoluteMinimum absolute minimum of the node AbsoluteMaximum absolute maximum of the node ArithmaticMean mean of the values at the node Discontinuity discontinuity based on discontinuity option -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-