ResultComplex Enumeration

NXOpen.CAE.Result.Complex is an alias for NXOpen.CAE.ResultComplex

class NXOpen.CAE.ResultComplex

Bases: object

Complex options

Enum Members

Enum Member Enum Member Description
Real
Imaginary
Amplitude
SignedAmplitude
PhaseAngle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.