VelocityImpactParametersStartPositionType Enumeration¶
NXOpen.CAE.ResponseSimulation.VelocityImpactParameters.StartPositionType is an alias for NXOpen.CAE.ResponseSimulation.VelocityImpactParametersStartPositionType
-
class
NXOpen.CAE.ResponseSimulation.
VelocityImpactParametersStartPositionType
¶ Bases:
object
the calculation start position for impact
Enum Members
Enum Member Enum Member Description AtDrop Calculation starts from the drop time BeforeImpact Calculation ends at the impact time AtImpact Calculation starts from the impact time -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-