VelocityImpactDirectionNodalComponentType Enumeration

NXOpen.CAE.ResponseSimulation.VelocityImpactDirection.NodalComponentType is an alias for NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionNodalComponentType

class NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionNodalComponentType

Bases: object

the types of nodal component

Enum Members

Enum Member Enum Member Description
Dof1
Dof2
Dof3
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.