VelocityImpactDirectionDirectionType Enumeration

NXOpen.CAE.ResponseSimulation.VelocityImpactDirection.DirectionType is an alias for NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionDirectionType

class NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionDirectionType

Bases: object

the direction options for impact

Enum Members

Enum Member Enum Member Description
NodalComponent
UserDefined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.