StrengthStressOption Enumeration

class NXOpen.CAE.ResponseSimulation.StrengthStressOption

Bases: object

The options of stress Enum Members

Enum Member Enum Member Description
ElementMaximum
NodeOnElement
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.