SolutionCollection Class¶
-
class
NXOpen.CAE.ResponseSimulation.
SolutionCollection
¶ Bases:
object
Represents a collection of response analysis meta solution
To obtain an instance of this class, refer to
NXOpen.CAE.ResponseSimulation.Manager
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ActiveSolution | Returns or sets the active solution |
Methods¶
Method | Description |
---|---|
CloneSolution | Clones a response analysis meta solution |
CreateSolutionBuilder | Creates the builder object of response analysis meta solution |
FindObject | Finds a response analysis meta solution with specified solution name |
Property Detail¶
ActiveSolution¶
-
SolutionCollection.
ActiveSolution
¶ Returns or sets the active solution
-------------------------------------
Getter Method
Signature
ActiveSolution
Returns: Return type: NXOpen.CAE.ResponseSimulation.Solution
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ActiveSolution
Parameters: activeSolution ( NXOpen.CAE.ResponseSimulation.Solution
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
CloneSolution¶
-
SolutionCollection.
CloneSolution
¶ Clones a response analysis meta solution
Signature
CloneSolution(oldSolution, suggestedName)
Parameters: - oldSolution (
NXOpen.CAE.ResponseSimulation.Solution
) – theCAE.SimSolution
to be cloned - suggestedName (str) – name to use instead of default name (may be NULL)
Returns: the newly created
CAE.ResponseSimulation.Solution
Return type: New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
- oldSolution (
CreateSolutionBuilder¶
-
SolutionCollection.
CreateSolutionBuilder
¶ Creates the builder object of response analysis meta solution
Signature
CreateSolutionBuilder(raSolution)
Parameters: raSolution ( NXOpen.CAE.ResponseSimulation.Solution
) –Returns: Return type: NXOpen.CAE.ResponseSimulation.SolutionBuilder
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
FindObject¶
-
SolutionCollection.
FindObject
¶ Finds a response analysis meta solution with specified solution name
Signature
FindObject(solutionName)
Parameters: solutionName (str) – Returns: Return type: NXOpen.CAE.ResponseSimulation.Solution
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)