SensorCoordinateType Enumeration

class NXOpen.CAE.ResponseSimulation.SensorCoordinateType

Bases: object

Specifies the coordinate type of Sensor Enum Members

Enum Member Enum Member Description
NodalCs
GlobalCs
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.