ResponseDomainDefinitionMethod Enumeration

class NXOpen.CAE.ResponseSimulation.ResponseDomainDefinitionMethod

Bases: object

Specifies response result evaluation options Enum Members

Enum Member Enum Member Description
StartEndPoint
KeyIn
NaturalFrequency
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.