RSEventSolverParameters Class¶
-
class
NXOpen.CAE.ResponseSimulation.
RSEventSolverParameters
¶ Bases:
NXOpen.TaggedObject
Represents a response analysis event
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DdamCoefficientA | Returns or sets the DDAM A coefficient |
DdamCoefficientV | Returns or sets the DDAM V coefficient |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetDdamCoefficient | Returns DDAM coefficient value of the specified type |
SetDdamCoefficient | Sets the DDAM coefficient value of the specified type |
Enumerations¶
RSEventSolverParametersDdamCoefficientType Enumeration | Represents DDAM coefficient type |
Property Detail¶
DdamCoefficientA¶
-
RSEventSolverParameters.
DdamCoefficientA
¶ Returns or sets the DDAM A coefficient
-------------------------------------
Getter Method
Signature
DdamCoefficientA
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
DdamCoefficientA
Parameters: coefficientA (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
DdamCoefficientV¶
-
RSEventSolverParameters.
DdamCoefficientV
¶ Returns or sets the DDAM V coefficient
-------------------------------------
Getter Method
Signature
DdamCoefficientV
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
DdamCoefficientV
Parameters: coefficientV (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
GetDdamCoefficient¶
-
RSEventSolverParameters.
GetDdamCoefficient
¶ Returns DDAM coefficient value of the specified type
Signature
GetDdamCoefficient(coefficientType)
Parameters: coefficientType ( NXOpen.CAE.ResponseSimulation.RSEventSolverParametersDdamCoefficientType
) –Returns: Return type: float New in version NX7.5.2.
License requirements: None.
SetDdamCoefficient¶
-
RSEventSolverParameters.
SetDdamCoefficient
¶ Sets the DDAM coefficient value of the specified type
Signature
SetDdamCoefficient(coefficientType, coefficient)
Parameters: - coefficientType (
NXOpen.CAE.ResponseSimulation.RSEventSolverParametersDdamCoefficientType
) – - coefficient (float) –
New in version NX7.5.2.
License requirements: nx_response_anlys (“NX Response Analysis”)
- coefficientType (