NodalFunctionExcitationType Enumeration

NXOpen.CAE.ResponseSimulation.NodalFunctionExcitation.Type is an alias for NXOpen.CAE.ResponseSimulation.NodalFunctionExcitationType

class NXOpen.CAE.ResponseSimulation.NodalFunctionExcitationType

Bases: object

the subtype of nodal function excitation

Enum Members

Enum Member Enum Member Description
NodalForce
EnforcedMotion
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.