NodalFunctionEvalRequest Enumeration

class NXOpen.CAE.ResponseSimulation.NodalFunctionEvalRequest

Bases: object

Specifies response request for nodal function evaluation Enum Members

Enum Member Enum Member Description
UserDefinedDirection
DataComponent
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.