NodalAveragingOption Enumeration

class NXOpen.CAE.ResponseSimulation.NodalAveragingOption

Bases: object

Specifies nodal averaging options Enum Members

Enum Member Enum Member Description
Shells
Solids
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.